RTD version update question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTD version update question

2,145件の閲覧回数
focusdoit
Contributor III

Hi Nxp experts,

I have a project created on RTD SW32K3_S32M27x_RTD_R21-11_4.0.0 on EB tresos, now I want to switch to RTD SW32K3_S32M27x_RTD_R21-11_4.0.0_P19.

Can I just replace the old link file SW32K3_S32M27x_RTD_R21-11_4.0.0.link with the new link file SW32K3_S32M27x_RTD_R21-11_4.0.0_P19.link?

Thanks

0 件の賞賛
返信
3 返答(返信)

2,120件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @focusdoit 

During the installation of the .exe, you can select the EB Tresos installation directory or you can copy all "<mod>_TS_T40D34M40I0R0" directories and .JAR files to the "<Tresos Install Path>\plugins" directory.

 

B.R.

VaneB

0 件の賞賛
返信

2,117件の閲覧回数
focusdoit
Contributor III

I mean the modules configured on old RTD, such as, Adc.xdm, Dem.xdm, Dio.xdm, Spi.xdum .. etc, can switch these configurations  to the new RTD smoothly?

0 件の賞賛
返信

2,082件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @focusdoit 

The project maintains the files from the previous version. I am afraid that it will be required to create a new project with the new RTD version. 

0 件の賞賛
返信