RTD version for S32K3 microcontrollers that supports Fls component

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD version for S32K3 microcontrollers that supports Fls component

Jump to solution
720 Views
Djuric
Contributor III

Hello,

What is the latest RTD version for K3 microcontrollers, specifically S32K344, that has a Fls component?
I have a problem in source code with backward compatibility, because Fls is now divided into two components.

I see that the Fls component is present in S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02, and not in S32K3_M27X Real-Time Drivers Version 3.0.0 P07

Q1:   Are there any RTD driver versions between these two that have a Fls component ?

Q2:   Which FS26 SBC AUTOSAR drivers is compatible with S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 ?

Tags (1)
0 Kudos
Reply
1 Solution
699 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric

In Autosar R21-11, the Fls Driver has been replaced by Mem_InFls/Mem_ExFls. RTD 3.0.0 P07 is ASR 4.7 (R21-11) compliant, while P01 is ASR 4.4. The latest RTD package which still contains the Fls component is S32K3_S32M27x Real-Time Drivers AUTOSAR 4.4 Version 4.0.0 P24.

Q1. I'm guessing you mean between P01 and P07? Unfortunately, there is not.

Q2. I'm not sure if there is a specific package, as the only ones I've seen only support 3.0.0 P07. Since I mainly support S32K3 devices, and not FS26 SBC, please enter another post (or a case) so an engineer from the analog team can support you instead.

Best regards,
Julián  

View solution in original post

2 Replies
688 Views
Djuric
Contributor III

Thank you for your answer.

0 Kudos
Reply
700 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Djuric

In Autosar R21-11, the Fls Driver has been replaced by Mem_InFls/Mem_ExFls. RTD 3.0.0 P07 is ASR 4.7 (R21-11) compliant, while P01 is ASR 4.4. The latest RTD package which still contains the Fls component is S32K3_S32M27x Real-Time Drivers AUTOSAR 4.4 Version 4.0.0 P24.

Q1. I'm guessing you mean between P01 and P07? Unfortunately, there is not.

Q2. I'm not sure if there is a specific package, as the only ones I've seen only support 3.0.0 P07. Since I mainly support S32K3 devices, and not FS26 SBC, please enter another post (or a case) so an engineer from the analog team can support you instead.

Best regards,
Julián