RTD Usage Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD Usage Issues

658 Views
NXP2
Contributor II

Hello, there are some issues when using the RTD project. Could you please take a look at them?

(1)After importing the demo project, why is the board.txt file empty? When compiling, there was an immediate error message. How can I compile the demo project?

NXP2_0-1787586202293.png

NXP2_1-1787586227880.png

(2)When I tried to open the .mex file of the demo project using S32DS, the following problem occurred. Could you please tell me how to fix it?

NXP2_0-1787585984659.png

 

Tags (1)
0 Kudos
Reply
3 Replies

631 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

导入S32K RTD的工程请点击File -> New -> S32DS Project From Example

RTD工程里有个/description.txt文件需要阅读,其中就有提到需要在外设工具里点击Update Code按钮然后再编译:

3.1 Generating the S32 configuration

Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).

Clicking on any one of those will generate all the components. Make the desired changes (if any) then click on the "S32 Configuration Tool->Update Code" button.

最后那张图片太模糊了完全看不清,需要你重新上传。发图片不建议直接黏贴到帖子里,建议使用 Insert Photos 按钮插入图片或者当附件上传也行。

S32DSv3.6.x里安装RTD的方法以及如何导入工程等,可以看一下该视频:How To Download, Install and Configure the RTD 5.0.0 with S32 Design Studio 3.6.0

Best Regards,
Robin

0 Kudos
Reply

498 Views
NXP2
Contributor II

Hi:
Thank you for your explanation. Currently, I am using the S32K1 series RTD. I have successfully installed RTD 3.0.0 using S32DS 3.6.0. I have successfully run the example project in RTD. However, when I try to create a new project, there is no SDK available to choose from. Why is that?

Snipaste_2026-09-06_02-06-24.pngSnipaste_2026-09-06_02-06-58.pngSnipaste_2026-09-06_02-08-19.png

 

0 Kudos
Reply

474 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

When creating an RTD project, please select the Compiler Options in the Toolchain that match those in the RTD release note. For example, you should select NXP GCC 10.2.0 instead of NXP GCC 11.4.

S32K1 RTD toolchain Compiler Options.png

0 Kudos
Reply