RAppID_BL via Vector CANCaseXL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID_BL via Vector CANCaseXL

2,638 Views
narudoltatiyava
Contributor I

Dear Sir,

 

I am trying to flash the simple FlexCAN0 project *.SREC file over CAN bus via GUI of RAppID_BL.

The hardware board is customized with S32K144 LQFP-64, normal functional tested via PEmicro flashed.

 

SREC build Pre-Test :

1) Complied the FlexCAN0 project modified from example to send out CAN in PTC2 & PTC3 instead. 

2) Flashed via PEmicro tested it work fine.

 

RBL configuration :

[FORMAT_VERSION]
3

[COMMUNICATION_SETUP]
Vector CANcaseXL, CH 1, 500K

[MCU_SETUP]
S32K144

[BAM_SETUP]
Disabled

[FILE_INFO]
C:\SVN_Checkout\S32DS_ARM2.2\S32K144_Project_FlexCan\Debug\S32K144_Project_FlexCan.srec, 0x0, 0x950, Checked

[OP_SETUP]
EraseProgram

 

CAN Flash Testing :

1) Load RBL file - C:\Freescale\RAppIDBL\RAppidBL_Vector_CANCaseXL.rbl

2) Error - Loss Communication

 

If any idea what setup I am doing wrongly ?

Or do you guy have any simple project working for testing

 

Best regards,

Narudol T.

0 Kudos
Reply
0 Replies