Questions about the random number generator function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the random number generator function

Jump to solution
2,764 Views
Derek_Yoon
Contributor I

Hello teams.

Hope all is well

I saw an NXP engineer's response to a TRNG related question on this board that "TRNG operates internally to generate the seed from which the PRNG is built."

So, does that mean there is no need to input a separate seed value to generate a random number?

 

Ps :  I know that when using the DRBG algorithm, it need to input a seed with a certain entropy. Are the DRBG algorithm and PRNG different concepts?

Tags (1)
0 Kudos
Reply
1 Solution
2,742 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Derek_Yoon 

Are we talking about CSEc on S32K1? It's given by SHE specification. Initial seed is generated by CMD_INIT_RNG command. Then you can generate random numbers while it is not necessary to reseed. The only additional thing you can do in runtime is to run CMD_EXTEND_SEED command to supply 128 bit of entropy. You can call this command whenever additional entropy is needed.

Regards,
Lukas

View solution in original post

0 Kudos
Reply
2 Replies
2,743 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Derek_Yoon 

Are we talking about CSEc on S32K1? It's given by SHE specification. Initial seed is generated by CMD_INIT_RNG command. Then you can generate random numbers while it is not necessary to reseed. The only additional thing you can do in runtime is to run CMD_EXTEND_SEED command to supply 128 bit of entropy. You can call this command whenever additional entropy is needed.

Regards,
Lukas

0 Kudos
Reply
2,724 Views
Derek_Yoon
Contributor I
That's right, I was asking about the CSEc on the S32K. Thanks for the help! My question is all cleared up
0 Kudos
Reply