Questions about flexcan id

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about flexcan id

2,127件の閲覧回数
Oido
Contributor III

I'm using s32k144w.
Can I get multiple IDs in RX with one buffer through FLEXCAN? For example, it is not a method of allowing IDs from 0x200 to 0x20f using RXIMR.
I wonder if it is possible to accommodate non-regular and non-consecutive IDs in one buffer like 0x225, 0x385, 0x448.
CAN0->RAMn[ 3*MSG_BUF_SIZE + 0] = 0xC4000000;
CAN0->RAMn[ 3*MSG_BUF_SIZE + 1] = 0x200<<18;//
CAN0->RXIMR[3] = 0x3f0<<18;

0 件の賞賛
返信
4 返答(返信)

2,089件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

If it is multiple random CAN IDs,then it is hard to do so.

0 件の賞賛
返信

2,083件の閲覧回数
Oido
Contributor III

Hello.Senlent
It's not random, it's fixed, but it's just not regular.
So you mean you have to use multiple buffers to use multiple IDs??
So S32K144W can use 7 buffers with 64 bytes, so you can only set up up to 7 IDs by combining TX and RX??

Wouldn't it be a problem if I set the RXIMR to 0x200 with one buffer and then get all the IDs and use only 0x201 and 0x600 of them?

CAN0->RAMn[ 3*MSG_BUF_SIZE + 1] = 0x200<<18;
CAN0->RXIMR[3] = 0x200<<18; 


RxID = ((CAN0->RAMN[ 3*MSG_BUF_SIZE + 1] & CAN_WMBn_ID_ID_MASK) >> 16);
if(RxID==0x201||RxID==0x600){
if((RxDATA3[1]&0x00000001)==0x00000001){
Direction = 0;
}
else if ((RxDATA3[1] & 0x00000002)==0x00000002){
Direction = 1;
}
}

Is there a problem with using it like this?

0 件の賞賛
返信

2,075件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

It's possible to do this, but take into account the data coming from the bus, if it's too much then you might lose frames

0 件の賞賛
返信

2,024件の閲覧回数
Oido
Contributor III

CAN0->RAMn[ 3*MSG_BUF_SIZE + 1] = 0x000<<18;
CAN0->RXIMR[3] = 0x000<<18;


RxID = ((CAN0->RAMN[ 3*MSG_BUF_SIZE + 1] & CAN_WMBn_ID_ID_MASK) >> 16);
if(RxID==0x201||RxID==0x600){
if((RxDATA3[1]&0x00000001)==0x00000001){
Direction = 0;
}
else if ((RxDATA3[1] & 0x00000002)==0x00000002){
Direction = 1;
}
}

 

Does this mean that if I set the RXIMR to 0x000 and get all the IDs and use only the data of the desired ID, I can get into trouble??
If so, is it recommended to use one in each buffer or a continuous range of IDs with RXIMR? I would appreciate it if you could elaborate.

0 件の賞賛
返信