Question about BCTU CL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about BCTU CL

2,470 Views
CKing
Contributor I

Hello,

In S32K3xx, if I want to do a sequence of conversion on one ADC, I can use BCTU CL to configure a sequence and BCTU will trigger ADC multiple times, or I can configure NCMRn/JCMRn to wait for a normal/injected trigger. Is the saying right?

Thanks

CK

0 Kudos
Reply
3 Replies

2,429 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi CK,

Sorry I may not understand your question.
Section 61.3.4.2 Operation modes in normal conversions of S32K3XXRM(Rev.7) mentions that you can use One-Shot mode or Scan mode to implement sequential conversion.

61.3.4.2 Operation modes in normal conversions sequential conversion.png

Section 65.3.2 Conversion list (CL) of S32K3XXRM mentions:
A CL executes a sequence of conversions on one or more target ADCs. It also stores information from the last conversion executed in a sequence except for the target ADC, which is stored in ADC select n (TRGCFG_m[ADC_SELn]).

65.3.2 Conversion list (CL) sequence of conversions.png

So I think either ADC normal conversions or BCTU CL can be used to sample a sequence of ADC channels.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,303 Views
CKing
Contributor I

Hi Robin,

Thanks for your information. I am curious about the flexibility to execute a sequence conversion.

Using CL to sample a sequence of channels is used in BCTU conversion mode. The BCTU conversion mode has the highest priority's trigger and sends one trigger to start one conversion in CL.

If I use NCMR/JCMR, only one trigger is required for a sequence conversion. However the sequence must follow the ascending order of channels to sample.

Therefore, there is not a way to start a sequence of normal conversion in any order which only requires a trigger. That is my question.

Thanks

CK

0 Kudos
Reply

2,268 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

61.3.4 Normal trigger 
Proceed through the standard input channels in ascending order.

61.3.4 Normal trigger in ascending order.png

Unfortunately I didn't find which register to start a sequence of normal conversion in any order which only requires a trigger.

0 Kudos
Reply