Pull-Up Resistor at GPIO Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pull-Up Resistor at GPIO Pin

2,021 Views
rak14
Contributor III

Hi,

I am using FS32K148UJT0VLUT Controller in my Project. The GPIO current drive is 20mA and less than that.

In one of the application we require a current drive of more than 20mA (around 50mA max). So, we thought of adding the external pull up resistor at the end of the GPIO pin which will give the more current drive to the DUT in use.

 

So, I wanted to know if we can add the pull up resistor at the end of the Push Pull or Open drain transistors.

The idea behind the current drive is added in the attachments, please do reply to the query asap.

 

Regards

0 Kudos
Reply
1 Reply

1,992 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Feel free to use any device to amplify or switch electrical signals and power but please make sure you are within the spec. For more details, see sections 5.3 or 5.4 of the datasheet.

Hope it helps you.

Have a nice day!

0 Kudos
Reply