Program partition command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program partition command

1,488 Views
814420552
Contributor III

Dear all, when I read mannual chapter 36.5.11.14 Program Partition command, has the following comment:

CAUTION

While different partitions of the FlexNVM are available, the intention is that a single partition choice is used throughout the entire lifetime of a given application. The FlexNVM Partition Code choices affect the endurance and data retention characteristics of the device .

what's the meaning of this this passage?

Tags (1)
0 Kudos
Reply
1 Reply

1,430 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Within the FlexNVM you have different partitions (data flash, emulated EEPROM, etc.), however, to increase the endurance and data retention characteristics of the device it's recommended that you use only a single partition. 

Best regards, 

Victor 

0 Kudos
Reply