Program a S32K from a 820A via SWD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program a S32K from a 820A via SWD?

1,654件の閲覧回数
perig_vennetier
Contributor I

Hello,

I'd like to setup an embedded system to be able to have a Snapdragon 820A program a S32K144 via SWD but it seems that 820A does not support SWD natively.

Anybody would have seen a solution to do the above?

Would there be a chip that can be the bridge between SPI and SWD for example?

Could any GPIO be used on the 820A to become a SWD channel by creating custom timing?

Thanks!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)