Program S32K142 Over CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program S32K142 Over CAN

Jump to solution
3,898 Views
JonnySchmidt
Contributor II

Hi,

I am trying to find a can bus supporting bootloader for the S32K142 (I'm currently working on the eval kit however this will soon be a custom solution). The application is automotive and the requirement is to be able to update the firmware remotely via can once the device is fitted and not easily accessible.

The application code is built using the model based design toolbox and the ideal solution to update the firmware is to have a (windows) gui in which to load the .elf file and set the application code start address and code size range, then program from the PC over can. For initial bootloader programming, programming over JTAG or by using the OpenSDA is acceptable.

It looks like the RAppID BL Tool is the best option, however the latest version (1.6.7.35) only supports the S32K144 under the MCU drop down menu. Is there an available bootloader for the S32K142 which would enable this use case?

Thanks

Jonny

0 Kudos
Reply
1 Solution
3,869 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jonny,

You can use the Unified Bootloader, it is ported to S32K142.

danielmartynek_0-1628692206219.png

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

 

Regards,

Daniel

 

View solution in original post

3 Replies
3,870 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jonny,

You can use the Unified Bootloader, it is ported to S32K142.

danielmartynek_0-1628692206219.png

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

 

Regards,

Daniel

 

3,860 Views
JonnySchmidt
Contributor II

Thanks Daniel,

Thanks, based on other posts in the community forums, I have now also raised a support ticket (00414468), requesting the NXP OpenBus software tool used to flash the chips as there's no download available.

Thanks

Jonny

0 Kudos
Reply
3,856 Views
JonnySchmidt
Contributor II

I've received the tool now via support. Thanks again for your help.

Jonny