Problems debugging with S32 Design Studio v3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems debugging with S32 Design Studio v3.4

Jump to solution
1,965 Views
VictorPastrana
Contributor III
Im experience some problems trying to debug a S32k3X4EVB-Q257 board
I follow the instructions on the Getting Started with the S32K3X4EVB-Q257 Evaluation Board | NXP Semiconductors, also double-check the colocation of the jumpers.
Im using a Segger J-Link Plus to try to debug it (also, i downloaded the Segger Commander just to verify if i can have some device recognition and apparently everything is correct)
VictorPastrana_0-1692828815518.png

 

Im trying to debug an SDK but im not able to accomplish that.
 
This is the error.
VictorPastrana_1-1692828835309.png

 

Here is the debugger configurations
VictorPastrana_2-1692828848273.pngVictorPastrana_3-1692828860381.pngVictorPastrana_4-1692828875167.pngVictorPastrana_5-1692828887476.png

 

 -Just in case this info is needed, im powering the board with external supply 12v.
-On the part of "Device Name", also change from CORTEX M7 to S32K344 and still have the same problem. 

0 Kudos
Reply
1 Solution
1,929 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to S32 Design Studio for S32 Platform V3.4/V3.5 + SEGGER J-LINK Plus


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,930 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to S32 Design Studio for S32 Platform V3.4/V3.5 + SEGGER J-LINK Plus


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply