Problem with receving using UART in s32k144 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with receving using UART in s32k144 board

905 Views
Ramsai
Contributor I

Hi,

Iam working on a project where I need to use UART for communication. while I tried the examples of the UART Iam able to transmit the data but not able to receive the data. 

While debugging I got to know that receive status is always busy.

Ramsai_0-1672303379654.png

Any suggestion to clear the issue?

MCU-S32K144

IDE-S32KDS 2.2V

Regards,

Ram

0 Kudos
Reply
1 Reply

886 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you refer to demo example (pluart_echo) it is written in the way the received chars are stored into user buffer and the reception stops when newline character (\n) is received or the buffer is full, then received data are echoed back. You can check if buffer is filled within debugger.

BR, Petr 

0 Kudos
Reply