I would like to set up the TPIU pins for trace but i have a problem that the pin PTD11 for Trace Data out 2 is already configured by ENET RMII Transmit Clock. ( PTC2 pin is also set up for RMII Transmit data 0)
Possible solutions are: either to use less data bits but then its likely/chance to lose data, or i can make both pins available in the PCB and only when programming ENET, i will use less trace data pins.
Any other solution to be able to trace ENET with all the trace 4 data pins ?
thanks!
Cheers,
Nader
Hello Nader,
Unfortunately, I don't see any other solution, all the pin functions can't be used at at the same time.
BR, Daniel
Hallo Daniel,
Ok thanks for the answer.
BR, Nader