Problem about installing RTM 3.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem about installing RTM 3.0.0

5,724 Views
Garam_Kim
Contributor I

 Hello

 I'm a beginner at this ARM processor and I installed S32 Design Studio for ARM Version 2018.R1 today

 And I downloaded S32DS_ARM_v2018.R1_UP9 to install the RTM 3.0.0 program and installed it using install new software from 'Help'. However, when creating new projects, only the 0.8.6 version is always available... I'd like to install the version of RTM 3.0.0 and I'd appreciate it if you could tell me how to fix the problem.

0 Kudos
Reply
3 Replies

5,715 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Garam_Kim,

s32ds 2008 is too old.
Newer IDE are recommend:
S32 Design Studio 3.3 with SDK S32K1xx RTM 4.0.0
OR
S32 Design Studio for ARM 2.2 with SDK S32K1xx RTM 3.0.3

You can install SDK by refer one of two article:
S32 Design Studio 3.3 - S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0 available!
S32 Design Studio for ARM 2.2 - Update 1 available

About how to install SDK3.0.0 in s32ds 2008, please refer: S32 Design Studio for ARM 2018.R1 - Update 9 available

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,722 Views
Garam_Kim
Contributor I

And i attach this picture that occurred Problem when i installed  S32 Design Studio S32K1xx RTM SDK 3.0.0 1.0.0.201902250553

0 Kudos
Reply

5,687 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please try to install latest update: S32 Design Studio for ARM v2018.R1 Update 11 with S32 SDK S32K1xx SR 3.0.2(REV UP11)
This version update S32 SDK S32K1xx RTM 3.0.0 with patch SR 3.0.2

If still doesn't work, then I recommend use new version S32 Design Studio.

0 Kudos
Reply