Problem Occurrend

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem Occurrend

5,189 Views
muggle
Contributor II

S32K144_64
multilink universal rev A

Run with Error starting process.
Cannot run program "D:\project\NXP\S32K144_V3.0.6_20241024\Debug_FLASH\DNB110X.elf": Launching failed
Cannot run program "D:\project\NXP\S32K144_V3.0.6_20241024\Debug_FLASH\DNB110X.elf": Launching failed
Cannot run program "D:\project\NXP\S32K144_V3.0.6_20241024\Debug_FLASH\DNB110X.elf": Launching failed

Debug with Error in final launch sequence
Failed to execute MI command:
-exec-run
Error message from debugger back end:
Error creating process D:\project\NXP\S32K144_V3.0.6_20241024\Debug_FLASH\DNB110X.elf, (error 193).
Error creating process D:\project\NXP\S32K144_V3.0.6_20241024\Debug_FLASH\DNB110X.elf, (error 193). 


How do I fix this?

0 Kudos
Reply
11 Replies

5,166 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@muggle

Could you please show us your Debug Configurations?

0 Kudos
Reply

5,140 Views
muggle
Contributor II

PE.jpgPE.jpg

Tags (1)
0 Kudos
Reply

5,130 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@muggle

Can you provide a screenshot of the entire configuration page?

It looks like you didn't start GDB but the elf file

0 Kudos
Reply

5,116 Views
muggle
Contributor II

11.jpg11.jpg22.jpg22.jpg33.jpg33.jpg44.jpg44.jpg55.jpg55.jpg66.jpg66.jpg77.jpg77.jpg

0 Kudos
Reply

5,103 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@muggle

There is no need to Configurate "C/C++ Application"

Senlent_0-1735866390372.pngSenlent_0-1735866390372.png

 

0 Kudos
Reply

5,099 Views
muggle
Contributor II

75.jpg75.jpg88.jpg88.jpg99.jpg99.jpg

0 Kudos
Reply

5,095 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@muggle

This prompt is very clear, no link detected
Are you using S32K144EVB? What debugger are you using?

你可以说中文

0 Kudos
Reply

5,091 Views
muggle
Contributor II

你好,非常感谢你的及时回复,我是初学者,我只知道这是S32K144,芯片上的标签是FS32K144H91.jpg91.jpg110.jpg110.jpg

0 Kudos
Reply

5,074 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@muggle

电脑显示你的PE应该是链接了,但是到MCU的链接没有正确,你确定你的调试器到MCU的连接是不是正确的,用J-LINK吗,可以用J-LINK也试一下。打开S32 DS提供的例程,直接编译烧写一个试一下。

0 Kudos
Reply

5,086 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@muggle

你确认下你的调试接口是不是正确,是SW口吗,你用的调试器是什么?是PE还是什么

0 Kudos
Reply

5,083 Views
muggle
Contributor II

JTAG,我是使用的是PE Multilink Universal Rev A

0 Kudos
Reply