Prevent the part of SDK code from being updated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Prevent the part of SDK code from being updated

384 Views
oguzhan1857
Contributor II

Hello,

I am currently using UART example with S32K3 RTD 4.0.0 P24 but I can't catch idle event because of Uart_Ipw_LpuartConvertEventType bug. I have to edit this function that inside Uart_lpw.c file but edited part does not remain permanently and even I change simulink function it replace Uart_lpw file with old one when click deploy button.

Is there way to protect this edited part ?
Also, the bug has been mentioned in this topic,
https://community.nxp.com/t5/S32K/S32K3-UART-IDLE-EVENT-BUG-RTD400/m-p/1862221

Tags (2)
0 Kudos
Reply
0 Replies