Peripheral tool code generation error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Peripheral tool code generation error

1,741 次查看
TWL
Contributor III


When I use S32DS for Platform 3.5 update (8) to configure a project for the S32K312 chip, after configuring peripherals and clicking to update the code, it shows errors with peripherals and clock. However, I'm using the default project, the clock hasn't been configured yet, and the peripherals are set to default values. The RTD version for S32K312 is 3.5.13.20240726.

TWL_0-1746511646458.pngTWL_0-1746511646458.pngTWL_1-1746511664975.pngTWL_1-1746511664975.png

 

0 项奖励
回复
4 回复数

1,716 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Even for newly created S32K312 project, there are default configurations in the Clocks Tool. Please enable code generation for Clocks.

S32 Configuration Tool Clocks.pngS32 Configuration Tool Clocks.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,698 次查看
TWL
Contributor III

The following image shows my operation. When I created a new project, I opened all code generation tools, and when I clicked update code, the following error was displayed.

TWL_0-1746670488449.pngTWL_0-1746670488449.png

TWL_1-1746670512020.pngTWL_1-1746670512020.png

 

 

0 项奖励
回复

1,695 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

First of all, I see that you installed S32K3 RTD 3.0.0 P01. But now it has been updated to 5.0.0. If it is a new project, it is recommended to use the latest version of RTD.
I did not encounter this error when creating a new project with S32DS v3.5 + RTD 3.0.0 P07. If you insist on using S32K3 RTD 3.0.0, then I suggest you uninstall this S32DS v3.5 and refer to this article to reinstall it HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

 

Best Regards,
Robin

0 项奖励
回复

1,674 次查看
TWL
Contributor III

Hi

I followed the steps you provided, but I'm still encountering the issue mentioned above.

TWL_0-1746681772011.pngTWL_0-1746681772011.png

 

0 项奖励
回复