Periodic timer Interrupt Priority configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Periodic timer Interrupt Priority configuration

1,837 Views
Dev15
Contributor III

Hello Team,

We have configured periodic timer interrupt (PIT) instance 0 with 4 channels in  S32 SDK configuration tool which are listed below

channel 0 (ISR 1)

channel 1 (ISR 2)

channel 2 (ISR 3)

channel 3 (ISR 4)

I'm trying to prioritize the ISR for above channels. Please help me in setting the priority for each of this channels

 

Thank you

Tags (1)
0 Kudos
Reply
2 Replies

1,719 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the late reply. Please post question in the S32K community next time. So that the internal system can assign your question to the engineer.

These four channel share the same Interrupt Priority, so you are not able to set different priorities for channels of an LPIT instance.

PIT interrupt Priority.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,710 Views
Dev15
Contributor III

@Robin_Shen ,

Thank you for your response.

I'm trying to create task schedulers based on priority levels say 1ms, 5ms, 10ms tasks.

Please let me know if any other sources available in s32k apart from PIT

 

0 Kudos
Reply