Pad keeping is not taking effect?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pad keeping is not taking effect?

Jump to solution
1,010 Views
PINKMAN
Contributor III

hello expert:

In my project, there is a wakeup source which is falling edge trigger. but  i can read it from   IP_WKPU->WISR even it doesn't happened.

before go to standby mode , i already enable Pad_Keeping by 

IP_DCM_GPR->DCMRWF1 &= ~DCM_GPR_DCMRWF1_STANDBY_IO_CONFIG_MASK;

after wakeup ,i disable it by 

IP_DCM_GPR->DCMRWF1 |= DCM_GPR_DCMRWF1_STANDBY_IO_CONFIG_MASK;

i think it should not happend in IP_WKPU->WISR 

can you tell me why ?

0 Kudos
Reply
1 Solution
991 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @PINKMAN,

I can see this is the same question as in this community post: WKPU->WISR and Pad_Keeping question - NXP Community.

I've replied to you there, is it okay to close this thread and keep support through the other one?

Best regards,
Julián

View solution in original post

0 Kudos
Reply
1 Reply
992 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @PINKMAN,

I can see this is the same question as in this community post: WKPU->WISR and Pad_Keeping question - NXP Community.

I've replied to you there, is it okay to close this thread and keep support through the other one?

Best regards,
Julián

0 Kudos
Reply