PTC2 pin cannot be pulled to 0 level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTC2 pin cannot be pulled to 0 level

Jump to solution
1,923 Views
FAR1234
Contributor III

Dear NXP experts,

I had PTC2 (yellow waveform) and PTE7 (blue waveform) ports periodically reverse, and found that PTC2 (yellow waveform) could not drop to 0V, as shown in the following figure.

FAR1234_0-1755699140494.png

The configuration parameters of PTC2 and PTE7 ports are as follows:

FAR1234_1-1755699343560.png

I look forward to your reply.

LF

 

0 Kudos
Reply
1 Solution
1,820 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @FAR1234 

It seems like your configuration is all set up correctly, and the issue is only happening with PTC2. Just to rule out any hardware-related issue, could you try routing the same signal to a different pin and see if the behavior changes?

It might also be worth taking a quick look at the PTC2 pin itself for any signs of physical damage or soldering issues.

View solution in original post

0 Kudos
Reply
5 Replies
1,884 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @FAR1234 

The S32K1xx Data Sheet (Rev. 14) defines VOH and VOL at specific current levels. If your circuit draws more current than allowed, the output voltage may not reach the expected high or low levels.

Also, not all pins have the same drive strength. Some are designed to handle more current. You should check the I/O characteristics section in the datasheet for details.

For a deeper understanding, I recommend looking at the “Output Characteristics” section in Application Note AN2434. Even though it is for the HCS12 family, it gives useful insights into how MCU pins behave.

 

BR, VaneB

0 Kudos
Reply
1,847 Views
FAR1234
Contributor III

Hi @VaneB 

I am glad to receive your reply.

Based on your suggestion, I have consulted relevant technical materials and conducted relevant tests, but the problem has not been resolved.

FAR1234_2-1755849826964.png

yellow waveform :PTC2;

blue waveform    : PTC3;

Let me add the background of my port usage:
My application is to configure PTC2 as FTM0_CH2 channel. Currently, this PTC2 pin is only connected to the oscilloscope probe and not to any other load, so there is no problem of output current exceeding the standard.
And it was me who configured the six channels of FTM0, only this FTM0_CH2 has a problem, while the other channels are normal.
I tried to increase the driving capability of PTC2 to a level of 20mA (as shown in the figure below), but the problem still persists.

FAR1234_0-1755849467932.png

FAR1234_1-1755849661423.png

Best regards

LF

 

 

0 Kudos
Reply
1,821 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @FAR1234 

It seems like your configuration is all set up correctly, and the issue is only happening with PTC2. Just to rule out any hardware-related issue, could you try routing the same signal to a different pin and see if the behavior changes?

It might also be worth taking a quick look at the PTC2 pin itself for any signs of physical damage or soldering issues.

0 Kudos
Reply
1,802 Views
FAR1234
Contributor III

Hi @VaneB 

I am glad to receive your reply.

I routed FTM0_C2 to PTD0, and the output of PTD0 is normal.

By carefully examining my development board, I found that PTC2 was connected to the CAN chip as CAN0-RX on the expansion board. After removing the CAN chip, PTC2 returned to normal.

Thank you very much for your guidance.

Best regards

LF

0 Kudos
Reply
1,909 Views
FAR1234
Contributor III
I would like to add that my MCU is S32K142W.
0 Kudos
Reply