PMC&CMU Error Injection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMC&CMU Error Injection

ソリューションへジャンプ
3,337件の閲覧回数
Pusoy
Contributor III

Hi,

Recently, I have been using the PMC and CMU modules, but I haven't found a way to inject related exceptions to validate my program logic.


1. For the PMC module, is there a way to inject voltage exceptions? (such as injecting high or low voltage exceptions for VDD_HV_A)
2. For the CMU module, is there a way to inject frequency exceptions? (such as injecting high or low frequency exceptions for CMU_FC0)


Thank you very much!

タグ(4)
0 件の賞賛
返信
1 解決策
3,218件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No PMC nor CMU injection is possible here. Nor required.

This is all covered by SAF:

petervlna_0-1704366956686.png

refer to safety manual for more details.

Best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,298件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

on certain microcotrollers there is, but please specify the device you are using.

Best regards,

Peter

0 件の賞賛
返信
3,236件の閲覧回数
Pusoy
Contributor III

Hello,

I have a development board based on the S32K344 chip, with the model S32K3x4_HDQFP172, as shown in the picture below.

1704280715718.jpg

Additionally, I also have a chip S32K312. 

1. Can these two devices inject PMC&CMU errors? If so, please provide the methods.

Thank you very much, I am looking for your replay!

0 件の賞賛
返信
3,219件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No PMC nor CMU injection is possible here. Nor required.

This is all covered by SAF:

petervlna_0-1704366956686.png

refer to safety manual for more details.

Best regards,

Peter

0 件の賞賛
返信
3,296件の閲覧回数
Pusoy
Contributor III

I am using S32K344 MQFP172

0 件の賞賛
返信