Hey NXP
I am using an S32K344 EVB Custom Board with a PEmicro Multilink Universe FX Rev-D
10-pin JTAG/SWD debug probe and S32 Design Studio (S32DS) version 3.6.8.
I would like to flash an application into the normal internal Program Flash of the S32K344.
I am not using HSE Secure Boot, Secure Debug, or any other security features which is not in our scop and not required for our Debug requirements.
currently I am facing the attached Issue while debugging so Your Immidiate guidence will help to resolve the issue in required fields
Could you someone please provide the detailed steps for:
- Connecting the PEmicro 10-pin JTAG/SWD debugger to the 10 Pin - S32K344 Custom EVB.
- Creating the correct Debug/Run configuration in S32DS 3.6.8.
- Selecting the proper interface (SWD or JTAG).
- Configuring flash programming settings (Erase, Program, Verify).
- Setting the correct target device and connection mode.
- Any required linker or memory configuration for standard internal flash programming.
- Recommended settings to avoid Secure Debug/HSE-related issues.
- Troubleshooting steps if the debugger detects the device but fails during flash programming.
I am looking for a complete flashing procedure and the exact S32DS configuration required for successful programming and debugging of the S32K344 EVB using a PEmicro probe.