PE Micro Multilink with MR-CANHUBK344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE Micro Multilink with MR-CANHUBK344

2,687 Views
ctunder77
Contributor I

Hello, 

   I am trying to program and debug the MR-CANHUBK344 board with a PE Micro Multilink LC and S32 Design studio. I am powering the board with 12V through P27 and the connections can be viewed in the image below. 

 

ctunder77_0-1699842275301.png

When I try to debug I get an error saying it was unable to connect the hardware. I have looked at some other posts for similar boards and delayed after reset by 300ms but I think the problem is the fact that debugger is not detecting any target voltage because the yellow LED isn't illuminated on the debugger. Is there a fix for this? Thanks in advance.

ctunder77_1-1699842331776.png

 

0 Kudos
Reply
4 Replies

2,516 Views
ctunder77
Contributor I

I have kept trying to debug with the PE micro multilink but I am still getting the following error when I try to debug.

ctunder77_0-1702612174753.png

 

This is my debugger configuration.

 

ctunder77_1-1702612234941.png

 

Can you please let me know what I am doing incorrectly?

 

0 Kudos
Reply

2,665 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, the yellow LED must be ON, so most probably there is issue with powering debugger.
You can try to measure pin1 of the connector to check voltage is present.

BR, Petr

0 Kudos
Reply

2,660 Views
ctunder77
Contributor I

Thank you for the reply. I have checked the voltage between 1(TVCC) on and pin 5(GND) and it is 3.3V. Shouldn't that be enough to cause the yellow light on the debugger to come on?

Thanks.

 

0 Kudos
Reply

2,636 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, it should. Check ribbon cable itself, connector placement and pin 1 alignment. You can also try to connect it directly to JTAG header on the board, P26.

BR, Petr

0 Kudos
Reply