NxpOpenBus and PCAN - .dll issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NxpOpenBus and PCAN - .dll issue

1,711件の閲覧回数
pawl
Contributor I

Hello,
I'm trying to use S32K144EVB with NxpOpenBus-win32-x64_v0.9 via the CANbus, using a PEAK PCAN-USB Pro. I am not able to 'Connect Device':
"FATAL ERROR! The underlying PCAN-Basic API (PCANBasic.dll) couldn't be certified..."

I found PCANBasic.dll in two locations:
1:
c:\windows\system32\PCANBasic.dll:
Verified: Signed
Description: PCAN-Basic API Library, x64
Product: PCAN-Basic API
Prod version: 4.8
File version: 4.8.1.872
MachineType: 64-bit
2:
c:\windows\syswow64\PCANBasic.dll:
Verified: Signed
Description: PCAN-Basic API Library, x86
Product: PCAN-Basic API
Prod version: 4.8
File version: 4.8.1.872
MachineType: 32-bit

Please help with this.

Thank you

0 件の賞賛
返信
1 返信

1,112件の閲覧回数
Tmon
Contributor I

Hi, I too have this problem. I'm using a PCAN-USB FD., with drivers 4.5.0.16741 with the PCAN-Basic API 4.9.0.942.  Have  you @pawl found a solution to this problem?

Tmon_0-1729113546229.png

0 件の賞賛
返信