Not able to flash using OpenSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to flash using OpenSDA

2,489 Views
anoop_radhakris
Contributor II

hi,

Iam using s32k144 evaluation board. After flashing an application related to watchdog Iam not able to debug the board using openSDA again. OpenSDA LED(D2) is OFF, LED(D3) is ON and the RESET LED(D1) is continuously ON. Also it is not able to detect the port for the interface(OpenSDA) used. Also Iam not able to enter the bootloader mode. Kindly suggest me  a solution to recover the board..

Regards,

Anoop 

0 Kudos
Reply
1 Reply

2,431 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Anoop,

Can you share the project?

Do you have any other debugger?

Thanks,

BR, Daniel

0 Kudos
Reply