Not able to flash using OpenSDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to flash using OpenSDA

2,575件の閲覧回数
anoop_radhakris
Contributor II

hi,

Iam using s32k144 evaluation board. After flashing an application related to watchdog Iam not able to debug the board using openSDA again. OpenSDA LED(D2) is OFF, LED(D3) is ON and the RESET LED(D1) is continuously ON. Also it is not able to detect the port for the interface(OpenSDA) used. Also Iam not able to enter the bootloader mode. Kindly suggest me  a solution to recover the board..

Regards,

Anoop 

0 件の賞賛
返信
1 返信

2,517件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Anoop,

Can you share the project?

Do you have any other debugger?

Thanks,

BR, Daniel

0 件の賞賛
返信