No source available for "(gdb[21].proc[42000].threadGroup[i1],gdb[21].proc[42000].OSthread[1])

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No source available for "(gdb[21].proc[42000].threadGroup[i1],gdb[21].proc[42000].OSthread[1])

1,305 次查看
995094985
Contributor I

lpuart_echo_s32k144 

This project was changed to 64 pin chip. This error will occur when downloading flash.

It works when downloaded to RAM.

0 项奖励
回复
1 回复

1,293 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

I'm able to download this example with a 64 pin package option without any error into a flash (I have only 100 pin package of S32K144). I have used S32DS for ARM 2018.R1 and selected 64 pin package. Please, try to use the attached code.

 

I hope it helps.

Best regards,

Diana

0 项奖励
回复