No rule to make target '{BaseProjDir}/Project_Settings/Linker_Files/S32K312_flash.ld' needby by

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No rule to make target '{BaseProjDir}/Project_Settings/Linker_Files/S32K312_flash.ld' needby by

1,144 Views
sam-azak
Contributor I

Hi All,

I'm working on importing a project and converting it to a C++ project.  I did this by creating a new project and then using the "Convert to a C/C++ Project" option.  I've tried this on several projects and I always get the same error.  It is:

make: *** No rule to make target '{WorkSpaceDir}/CPPTest/Project_Settings/Linker_Files/S32K312_flash.ld', needed by 'CPPTest.elf'. Stop.

I've tried adjusting file paths and build paths but I can't seem to sort out the problem.  Is there a specific thing I need to change in the build variables.

Cheers,

Sam

 

Tags (1)
0 Kudos
Reply
3 Replies

1,128 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @sam-azak,

Unfortunately, the RTD packages are not compatible with C++. S32DS is not determined for creating generic C/C++ project. S32DS is determined for projects related to specific microcontroller with the required SDK/RTD (S32DS Project > select appropriate microcontroller).

The option for a C++ project is available only because S32DS is based on Eclipse, so it is not recommended creating project this way in S32DS at all.

There are some workarounds, (like you mentioned, converting the project to C++ after importing the RTD package) but the functionality is not guaranteed, you can see some discussions about the topic below:

You can try some solutions from those links. Specifically, the second thread talks about the linker file when generating C++ projects
 
Best regards,
Julián
0 Kudos
Reply

1,068 Views
sam-azak
Contributor I

Hi @Julián_AragónM,

I appreciate the response!  I actually got a little further and no longer am getting the same error.  This was by following the tutorial on the Eclipse forum that you shared.  I think I just needed to change the startup code to be a cpp file.

I'm a little confused when you say the RTD packages are not compatible with C++.  In all of the RTD header files in my project, there is linkage to C when compiling a C++ application.  They all have the following:

#ifdef __cplusplus
extern "C"{
#endif

////// File Code

#ifdef __cplusplus
}
#endif

 

With some of the other controllers I've used, the driver code uses similar linkage and I've always assumed that this is how the library are compatible with C.  And at this point, I'm actually able to build the code without and errors or warnings!

However, when I try run the code with the debugger, I'm getting a new error.  The debugging session starts, and then there seems to be errors with the Disassembly process.  In the Disassemble window in S32DS, it shows:

fffffff6:   movs    r0, r0
fffffff8:   movs    r0, r0
fffffffa:   movs    r0, r0
fffffffc:   movs    r0, r0
fffffffe:   movs    r0, r0
100000000:   Unable to retrieve disassembly data from backend.
100000001:   Unable to retrieve disassembly data from backend.
100000002:   Unable to retrieve disassembly data from backend.
100000003:   Unable to retrieve disassembly data from backend.
100000004:   Unable to retrieve disassembly data from backend.
100000005:   Unable to retrieve disassembly data from backend.
100000006:   Unable to retrieve disassembly data from backend.
100000007:   Unable to retrieve disassembly data from backend.


Where as when I compile the same project in C the memory seems to be filling in a little more as I would expect:

569           ldr r3, =ITCM_DECOUPLE_END
20400210:   strh    r0, [r0, #0]
20400212:   movs    r0, r0
584           ldr  r0, =RESET_CATCH_CORE
20400214:   strb    r0, [r6, r5]
20400216:   movs    r0, #64 @ 0x40
597           ldr  r0, =__Stack_dtcm_start
20400218:   movs    r0, r0
2040021a:   movs    r0, #1
731           ldr  r0, =MSCM_CPXNUM
2040021c:   movs    r4, r0
2040021e:   ands    r6, r4
747       ldr  r1, =__RAM_INTERRUPT_START
20400220:   movs    r0, r0
20400222:   movs    r0, #0
66        {
          main:
20400224:   push    {r3, lr}
68            Clock_Ip_Init(clockConfig);
20400226:   ldr     r0, [pc, #40]   @ (0x20400250 <main+44>)
79                if (1U == toggleLed)
20400228:   ldr     r4, [pc, #40]   @ (0x20400254 <main+48>)
68            Clock_Ip_Init(clockConfig);
2040022a:   bl      0x20400ea8 <Clock_Ip_Init>
81                    Siul2_Dio_Ip_TogglePins(LED_PORT, (1UL << LED_PIN));
2040022e:   ldr     r5, [pc, #40]   @ (0x20400258 <main+52>)
70            Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals,g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals);
20400230:   movs    r0, #1

 

Do you know why I would be having these errors when trying to run the project in C++?  My hunch has to do with the linker files, but I've never needed to modify these before.

Thanks,

Sam

0 Kudos
Reply

1,055 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @sam-azak,

Have you tried to configure the linker file after converting the project?

Navigate to C/C++ Build > Settings.
Under Tool Settings, find the C++ Linker section.
Add any necessary libraries and paths in the Libraries and Library search path sections.

You can also try to add the linker file manually, as shown in this post: Solved: C/C++ S32DS Project - NXP Community.

That said, C++ implementation is unfortunately out of this community's scope of support.

Best regards,
Julián

0 Kudos
Reply