Need information Regarding CANFD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need information Regarding CANFD

1,423 Views
pratayay123
Contributor III

Dear Team,

How to implement CAN FD in S32K144EVB eval kit and pls share if there any Sample code for CANFd using S32K144EVB kit.

Thanks,

Pratyay

0 Kudos
Reply
1 Reply

1,402 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@pratayay123

          There is sample code "flexcan_encrypted_s32k144" in S32 DS ,which show you the usage of  the FlexCAN module configured to use Flexible Data Rate.

Usage or detail please refer to “flexcan_encrypted.dox” in project Doxygen file.

BR!

     Jim,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply