Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx

5,155 Views
marotib
Contributor I

Currently in my project :  CAN Instance 0 is used for DAQ in normal mode ,CAN Instance 1 is used for PTCAN in normal mode and CAN instance 2 is used for PTCAN in listen only mode.

Now we are able to set CAN HW filters on CAN_0 and everything working as expected but we are unable to set CAN HW filters on instance CAN_1 and CAN_2.

In configuration tool --> enhanced rxfifo configuration option is disable for both the instance 1 & 2 and If I try to do the same through software then init getting fail.

So please let me know the way to set enhanced rxfifo.

 

                      

0 Kudos
Reply
3 Replies

5,135 Views
marotib
Contributor I

Hello BR, Petr ,

If possible can you suggest solution to achieve below requirement

>configure HW filters with CAN-FD.

 I m using S32K344

0 Kudos
Reply

5,132 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

5,137 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you did not specify a device, but most probably an Enhanced RXFIFO is not available for used instances.
Refer to chapter 74.1 Chip-specific FlexCAN information of the device RM for implementation.

BR, Petr

0 Kudos
Reply