Need explanation for Trigger mux hardware input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need explanation for Trigger mux hardware input

1,052 Views
kyf
Contributor V

Hello NXP team!

 

Can you please someone explain to me what exactly items noted in the image bellow (1, 2) represent ?

I've opened MCL driver manual but still, I could not understand which signals are the ones in the image.

 

eMios_ReloadOut_vs_IPP__TRGMuxHWinput.jpg

1. What is "RELOAD_OUT" ?

2. What is "IPP" ?

3. Where are the two options described in the documentation ?

 

 

Kind regards,

kyf

0 Kudos
Reply
1 Reply

1,039 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @kyf 

VaneB_0-1672957712267.png

eMIOS_n_ipp_ind_emios_ch[ ] is the input to the eMIOS from the TRGMUX and eMIOS_n_ipp_do_emios_ch[ ] is the output of the eMIOS to the TRGMUX. For eMIOS_n_reload_out_ch[ ], eMIOS provides reload outputs,

To summarize they are simply input/output of eMIOS.

Regarding the image you post, these definitions are the value for the trigger selection logic of the TRGMUX module.

VaneB_1-1672960585818.png

 

B.R

VaneB

 

 

0 Kudos
Reply