Need LPI2C example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
11,100件の閲覧回数
huaping
Contributor III

Need one LPI2C master mode working example, referring to the example under SD32 installation, it see can send out right data, but get the wrong data when receiving.  This LPI2C module is different with old Freescale MCU.

Thanks a lot!

ラベル(1)
0 件の賞賛
返信
1 解決策
10,119件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Assuming that you want to read a value from an address, in your case 0x8C, you need to modify the code to perform a repeated start instead of a stop-start sequence when writing the code. 

while(1)
{
for (i = 0u; i < TRANSFER_SIZE; i++)
{
buffer[i] = i;
}
buffer[0]=0x8C;
/* Send a packet of data to the bus slave */
LPI2C_DRV_MasterSendDataBlocking(FSL_LPI2C1,buffer,1, false /* Do not send stop after the transfer */, OSIF_WAIT_FOREVER);

/* Clear the buffer to prepare it for the next operation */

/* Request data from the bus slave */
LPI2C_DRV_MasterReceiveDataBlocking(FSL_LPI2C1, buffer, 3, true, OSIF_WAIT_FOREVER);

for(i=0;i<9999;i++);

}

Here is a snip with a read operation of some IC registers(I can confirm the validity of the data, since reading the WHO_AM_I register returned the expected data):

pastedImage_3.png

As for the callback name generation, you should replace in the lpi2c component lpi2c1_MasterCallback0 with NULL to avoid modifying it at every code generation.

Hope that this helps.

Best regards,

Rares

元の投稿で解決策を見る

0 件の賞賛
返信
11 返答(返信)
10,119件の閲覧回数
huaping
Contributor III

Dear Rares:

        I can't upload project, so I write one ticket in TIC for help.

        Pls help it!

Thanks!

0 件の賞賛
返信
10,122件の閲覧回数
huaping
Contributor III

Dear Bares:

        It's ok now!

        Thanks a lot!

Huaping

0 件の賞賛
返信
10,122件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Can you attach the project that is receiving wrong data? Also it would be useful to add the expected and received data.

Thank you,

Rares 

0 件の賞賛
返信
10,121件の閲覧回数
huaping
Contributor III

Hi, Bares:

     Pls help check my project, I just didn't use interrupt, and change the below codes, masterCallback =0;

const lpi2c_master_user_config_t lpi2c1_MasterConfig0 = {
  .slaveAddress = 127U,
  .is10bitAddr = false,
  .operatingMode = LPI2C_STANDARD_MODE,
  .baudRate = 100000U,
  .baudRateHS = 0U,
  .masterCode = 0U,
  .transferType = LPI2C_USING_INTERRUPTS,
  .masterCallback = 0,//lpi2c1_MasterCallback0,
  .callbackParam = NULL,
};

     Thanks a lot!

0 件の賞賛
返信
10,120件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Assuming that you want to read a value from an address, in your case 0x8C, you need to modify the code to perform a repeated start instead of a stop-start sequence when writing the code. 

while(1)
{
for (i = 0u; i < TRANSFER_SIZE; i++)
{
buffer[i] = i;
}
buffer[0]=0x8C;
/* Send a packet of data to the bus slave */
LPI2C_DRV_MasterSendDataBlocking(FSL_LPI2C1,buffer,1, false /* Do not send stop after the transfer */, OSIF_WAIT_FOREVER);

/* Clear the buffer to prepare it for the next operation */

/* Request data from the bus slave */
LPI2C_DRV_MasterReceiveDataBlocking(FSL_LPI2C1, buffer, 3, true, OSIF_WAIT_FOREVER);

for(i=0;i<9999;i++);

}

Here is a snip with a read operation of some IC registers(I can confirm the validity of the data, since reading the WHO_AM_I register returned the expected data):

pastedImage_3.png

As for the callback name generation, you should replace in the lpi2c component lpi2c1_MasterCallback0 with NULL to avoid modifying it at every code generation.

Hope that this helps.

Best regards,

Rares

0 件の賞賛
返信
10,120件の閲覧回数
huaping
Contributor III

Hi,Rares:

     The project was ok in DS V1.2, now we upgrade to V1.3, and find it is error when compile, then we find it is the reason when add the below code:

 LPI2C_DRV_MasterInit(FSL_LPI2C1, &lpi2c1_MasterConfig0,&lpi2c1MasterState);

     but this is necessary to do initial.

     Would you pls help check my project as attached?

     Thanks!

0 件の賞賛
返信
10,120件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi Huaping,

Can you attach the log of the failed build?

Best regards,

Rares

0 件の賞賛
返信
10,120件の閲覧回数
huaping
Contributor III

Dear Rares:

         May I know what version of DS you are using? V1.2 or V1.3?

         I change masterCallback = NULL, it is ok to compile, but the code always return back at the below codes:

lpi2c_master_state_t *master = g_lpi2cMasterStatePtr[instance];      // I can't find it where is used
if (master == NULL)
{
return LPI2C_STATUS_FAIL;           // it return for here
}

/* mark transfer as blocking */
master->blocking = true;

retVal = LPI2C_DRV_MasterSendData(instance, txBuff, txSize, sendStop);   // can't run here, if I delete the below codes, it will jump to ISR interrupt.

I don't know how to upload the project again, can't find it.

10,120件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi Huaping,

I suggest using S32 DS V1.3 as it is improved.

Are you calling the init function prior to using LPI2C_DRV_MasterSendDataBlocking? It seems that the driver is not initialized(g_lpi2cMasterStatePtr[instance] is configured in Init function).

You can attach the project by clicking on "Use advanced editor" on top-right corner when replying.

Best regards,

Rares

0 件の賞賛
返信
10,121件の閲覧回数
huaping
Contributor III

Dear Rares:

         Pls help check my project!

         thanks a lot!


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 件の賞賛
返信
10,120件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi Huaping,

Please find attached the project which was updated to fix the reported issues.

I had found the following issues which triggered the unwanted behaviour:

 1)   System OSC source was configured in Clock Manager to use External Reference. If you are using the DEVKIT, the source should be Internal Oscillator, as the input for the clock is retrieved from a crystal oscillator on PTB6 and PTB7 pins.

  2)   Functional clock for LPI2C was configured in PCC to use SPLLDIV2 which was disabled in the Clock Manager  component. Functional clock should be selected from an Async divider which is enabled.

  3) LPI2C baud rate was configured as 0. It should be greater than 0. Also selected pins for LPI2C were PTB7 and PTB6 which are used for Crystal input. I had routed SDA and SCL to PTA2 and PTA3.

Best regards,

Rares

0 件の賞賛
返信