NXP s32k116 example linkerscript and startup code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP s32k116 example linkerscript and startup code

2,970 次查看
MohameddRIAD
Contributor II

Hello,

I have installed an autosar package "SW32K1_RTD_4.4_1.0.1" and inside each plugin for example  "Adc_TS_T40D2M10I1R0" there exists a folder called examples and there is a folder for each s32k derivative   s32k118 , s32k144 , s32k144W ..etc. ,  the question is why there is no example for s32k116 this package is supposed to support s32k1xx as it was said also there are files configuration files with extension .epd that is for s32k116.  

My request is that I want an example linker script and startup code for s32k116 , why doesn't it exist in package ? can you provide me with one?

Best regards,
Mohamed.

0 项奖励
回复
5 回复数

2,929 次查看
MohameddRIAD
Contributor II

Hi,

Thank you for sharing the attachment. I will take a look and let you know if I have any further questions.

Also, would it be possible for you to share the startup code as well?

Thank you again for your help.

Best regards,


Mohamed.

0 项奖励
回复

2,920 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@MohameddRIAD

sure, 

If you have installed RTD, you can actually find the corresponding link and startup file in the following path

etc:

startup

C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K1_2022_02\SW32K1_RTD_4_4_1_0_1_D2202\Platform_TS_T40D2M10I1R0\startup\src

Senlent_0-1685609664051.png

Linker file

C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K1_2022_02\SW32K1_RTD_4_4_1_0_1_D2202\Platform_TS_T40D2M10I1R0\build_files\gcc

 

0 项奖励
回复

2,935 次查看
MohameddRIAD
Contributor II

Hi,

Thank you for your swift response , do you happen to have it in .icf extension to be compatible with IAR tool chain ? , also do you have a corresponding startup code with it ?

0 项奖励
回复

2,933 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@MohameddRIAD

please check the attachment,hope it works for you.

0 项奖励
回复

2,942 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@MohameddRIAD

I am attching it for your reference.

0 项奖励
回复