NXP s32k116 example linkerscript and startup code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP s32k116 example linkerscript and startup code

2,820件の閲覧回数
MohameddRIAD
Contributor II

Hello,

I have installed an autosar package "SW32K1_RTD_4.4_1.0.1" and inside each plugin for example  "Adc_TS_T40D2M10I1R0" there exists a folder called examples and there is a folder for each s32k derivative   s32k118 , s32k144 , s32k144W ..etc. ,  the question is why there is no example for s32k116 this package is supposed to support s32k1xx as it was said also there are files configuration files with extension .epd that is for s32k116.  

My request is that I want an example linker script and startup code for s32k116 , why doesn't it exist in package ? can you provide me with one?

Best regards,
Mohamed.

0 件の賞賛
返信
5 返答(返信)

2,779件の閲覧回数
MohameddRIAD
Contributor II

Hi,

Thank you for sharing the attachment. I will take a look and let you know if I have any further questions.

Also, would it be possible for you to share the startup code as well?

Thank you again for your help.

Best regards,


Mohamed.

0 件の賞賛
返信

2,770件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@MohameddRIAD

sure, 

If you have installed RTD, you can actually find the corresponding link and startup file in the following path

etc:

startup

C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K1_2022_02\SW32K1_RTD_4_4_1_0_1_D2202\Platform_TS_T40D2M10I1R0\startup\src

Senlent_0-1685609664051.pngSenlent_0-1685609664051.png

Linker file

C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K1_2022_02\SW32K1_RTD_4_4_1_0_1_D2202\Platform_TS_T40D2M10I1R0\build_files\gcc

 

0 件の賞賛
返信

2,785件の閲覧回数
MohameddRIAD
Contributor II

Hi,

Thank you for your swift response , do you happen to have it in .icf extension to be compatible with IAR tool chain ? , also do you have a corresponding startup code with it ?

0 件の賞賛
返信

2,783件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@MohameddRIAD

please check the attachment,hope it works for you.

0 件の賞賛
返信

2,792件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@MohameddRIAD

I am attching it for your reference.

0 件の賞賛
返信