NXP: S32k144: LPUART: RX upon interrupt does not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP: S32k144: LPUART: RX upon interrupt does not work

2,095 次查看
ArSa
Contributor II
Hello NXP,
I am having an issue with LPUART Rx via interrupt,

I have used following code using the macros from library header file s32K144.h,


The Tx works perfectly fine, But Rx is recieved with garbage. There is an obeservation

that RDRF bit gets disables before we read DATA register. I am not sure how this is related to
my issue but It seems incorrect for me though(as per RM Page 1707).

Please let help me in debugging the issue...

/************CODE STARTS HERE**********************/

/* Global static character */
uint8 static u8TxChar = 0u;
uint8 static u8RxChar = 0u;


void LPUART1_Init(void)
{

DISABLE_INTERRUPTS();

/* Step 1 : Enable Clock : 8Mhz Clk Init is used from the example project*/
PCC->PCCn[PCC_LPUART1_INDEX] &= ~PCC_PCCn_CGC_MASK; /* Ensure clk disabled for config */
PCC->PCCn[PCC_LPUART1_INDEX] |= PCC_PCCn_PCS(0b010) /* Clock src=2 (SIRCDIV2_CLK) */
| PCC_PCCn_CGC_MASK; /* Enable clock for LPUART1 regs */

/* Step 2 Initialize the Baud and CTRL, with SBR 0x11, and OSR 0x03000011
Tx Enable Rx Enable, RIE Enable*/

LPAURT1 -> BAUD = 0x03000011; /* 115200 Baud rate */
LPAURT1 -> CTRL = 0x002C0000;

/* Initialize interrupt */
S32_NVIC->ICPR[1u] = 1 << (LPUART1_RxTx_IRQn % 32); /* IRQ99 - FTM1 ch0,1: clear any pending IRQ*/
S32_NVIC->ISER[1u] = 1 << (LPUART1_RxTx_IRQn % 32); /* IRQ99 - FTM1 ch0,1: enable IRQ */
S32_NVIC->IP[LPUART1_RxTx_IRQn] = 0x00; /* IRQ99 - FTM1 ch0,1: priority 0 of 0-15*/

ENABLE_INTERRUPTS();

}

void LPUART1_TxChar(sint8 u8Char)
{

u8TxChar = u8Char;

LPAURT1 -> CTRL |= LPUART_CTRL_TIE(1u);

}

void LPUART1_RxTx_IRQHandler(void)
{

/* Tx Data */
if( TRUE == (((LPAURT1 -> STAT) & LPUART_STAT_TC_MASK ) >> LPUART_STAT_TC_SHIFT) )
{
/* Write into the Data register*/
LPUART1 -> DATA = u8TxChar;

/* Disable interrupt*/
LPAURT1 -> CTRL &= ~LPUART_CTRL_TIE_MASK;
}

/* Rx Data */
if(TRUE == (((LPAURT1 -> STAT) & LPUART_STAT_RDRF_MASK ) >> LPUART_STAT_RDRF_SHIFT ))
{
/* Write into the Data register*/
u8RxChar = LPUART1 -> DATA ;

}

}

/*****************CODE ENDS HERE***************************/
标记 (4)
0 项奖励
回复
1 回复

2,089 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi FrustatedEngineer,

Please refer the Example S32K144 LPUART RXEDGIF VLPS.
Hope it helps!

Example_S32K144_LPUART_RXEDGIF_VLPS.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复