NXP S32K14X Autosar OS error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP S32K14X Autosar OS error

4,320 Views
Simin
Contributor II

Hi,

        I configure an OS project with EB tresos for NXP S32K146 platform.

        I have install eb tresos “setup.exe”、“S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0.exe”、“JRE

6.0”, two errors will appear when verifying the project now,as below

1).The external generator for module Os_TS_T40D2M4I0R98 terminated with exit code 1:

         Simin_0-1629098210709.pngSimin_0-1629098210709.png

2).Failed to run generator "Os_TS_T40D2M4I0R98GeneratorId" (mode: "verify") for module "Os_TS_T40D2M4I0R98":

        Simin_1-1629098328275.pngSimin_1-1629098328275.png

        Pls provide help to solve these two errors,thanks very much for your kind support!

Best regards,

simin

 

 

 

0 Kudos
Reply
5 Replies

4,169 Views
JustVb
Contributor III

hello,have you solved it and could you share me the method? i met the same problem. the java environment is ok

JustVb_0-1639572850208.pngJustVb_0-1639572850208.pngJustVb_1-1639572864393.pngJustVb_1-1639572864393.pngJustVb_2-1639572879326.pngJustVb_2-1639572879326.png

 

0 Kudos
Reply

4,160 Views
namnguyenviet
NXP Employee
NXP Employee

hello,

You  should install  a 64-bit version of JRE. You can refer to this link: https://www.quora.com/How-do-you-know-if-youre-running-Java-in-32-bits-or-64-bits to know how to identify the JRE version.

Best Regards,

Nam

0 Kudos
Reply

4,145 Views
JustVb
Contributor III

hello, thx for your relay, I changed the JRE into 64-bit but the problem not solved

JustVb_0-1639625916726.pngJustVb_0-1639625916726.png

 

0 Kudos
Reply

4,129 Views
namnguyenviet
NXP Employee
NXP Employee

Then I'm not sure what could be the issue. Please try to install the SW in a new PC and see whether the issue persist.

Best Regards,

Nam

0 Kudos
Reply

4,303 Views
namnguyenviet
NXP Employee
NXP Employee

You can refer to this thread: https://community.nxp.com/t5/MPC5xxx/How-to-run-MPC574xG-AUTOSAR-OS-with-EB-software/m-p/1210219#M17...

https://community.nxp.com/t5/S32K/AUTOSAR-OS-S32K1/m-p/1155195

Check whether the java has been installed in system environment path, and try with command line.

0 Kudos
Reply