Hi Dears.
My custom board is not work after my code is run the error message is
ERROR: Can not read register (xx) while CPU is running.
xx : 0 ~ 16
I can download my code to my custom board with J-Link debugger.
But I can't set breakpoint after the code is run.
I read some others have same problem but I can't find how to solve it.
MCU : S32K312
IDE : S32DS for S32 Platform Version 3.4
Debugger J-Link Pro (GDB Server V7.82)
Thaks.
Thanks for VaneB
I read your comment and I did trace to find where make this problem. I find at Port_Ipw_Init_UnusedPins in Port_Init.
So I did make workaround that the JTAG_TDO pin config to JTAG_TDO without no configuration.
After that my debugger start to run and I also can set breakpoint.
Thanks.
Hi @dnewbe
Please verify the connections of the debug, for this take a look to the schematic of the S32K312EVB-Q172: S32K312EVB-Q172 Evaluation Board Design Files
Also, this community post will be useful for you: Design Considerations for Debug
B.R.
VaneB