Multiple timer functions in same FTM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiple timer functions in same FTM

977 次查看
Mudkip
Contributor I

I want to use one FTM channel as PWM output, and another one for IC, both signals are the same frequency so, the MOD register wont be an issue.

Basically I want to compare the output PWM with what is being captured, this signal goes through other boards and eventually comes back.
Is there a way of checking that the period and phase are the same?
Right now I cannot configure the FTM to work in both modes. Also, I know FTM doesn't support phase comparison but I found a workaround for that one.

I have read this, but this one if for OC mode: Use-an-FTM-IC-device-to-set-several-channels-as-output-compare 



 

 

0 项奖励
回复
1 回复

950 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

I must admit that it is not completely clear your request. What do you mean with checking the phase?

The FTM capture mode can determine the pulse width or the period of the tested signal but not both of them at the same time.

Have a nice day!

0 项奖励
回复