Multiple definition error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiple definition error

9,469 次查看
AbhijithKannan
Contributor II

I am new NXP and am currently learning how to you use. I want use UART to send message to desktop using USB2TTL converter. I enable lpuart peripheral in code configurator and updated the code as given below. When I compile the code I get multiple definition error.

Board : S32K1446 EVAL BRD

IDE : S32 Design Studio Platform 3.5

/*!
 ** Copyright 2020 NXP
 ** @file main.c
 ** @brief
 **         Main module.
 **         This module contains user's application code.
 */
/*!
 **  @addtogroup main_module main module documentation
 **  @{
 */
/* MODULE main */

/* Including necessary configuration files. */
#include "sdk_project_config.h"
#include "interrupt_manager.h"
#include "clock_config.h"
#include "peripherals_lpuart_1.h"
#include "pin_mux.h"

volatile int exit_code = 0;
/* User includes */

#include <stdio.h>
#define LED0_PORT PTD
#define LED0_PIN  15

#define LED1_PORT PTD
#define LED1_PIN  16

#define LED2_PORT PTD
#define LED2_PIN  0

#define GPIO_OUT_PORT PTD
#define GPIO_OUT_PIN  18
#define SW3_PIN  13
#define SW2_PIN  12

volatile uint8_t count = 0;

void delay(volatile int cycles) {
	/* Delay function - do nothing for a number of cycles */
	while (cycles--)
		;
}
uint32_t UART1;
void PORTC_ISR(void) {

	uint32_t status = PINS_DRV_GetPortIntFlag(PORTC);

	if ((status >> SW3_PIN) & 0b1) {
		count++;
		PINS_DRV_ClearPinIntFlagCmd(PORTC, SW3_PIN);

	}
	if ((status >> SW2_PIN) & 0b1) {
		PINS_DRV_ClearPinIntFlagCmd(PORTC, SW2_PIN);
		count++;
	}
	if (count >= 4) {
		count = 0;
	}
	char uartbuf[100];
	sprintf(uartbuf, "Count status : \n", count);
	LPUART_DRV_SendDataBlocking(&UART1, uartbuf, strlen(uartbuf), 3000);
}

/*!
 \brief The main function for the project.
 \details The startup initialization sequence is the following:
 * - startup asm routine
 * - main()
 */
int main(void) {
	/* Write your code here */
	status_t error;
	/* Configure clocks for PORT */
	error = CLOCK_DRV_Init(&clockMan1_InitConfig0);
	DEV_ASSERT(error == STATUS_SUCCESS);
	/* Set pins as GPIO */
	error = PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
	DEV_ASSERT(error == STATUS_SUCCESS);
	INT_SYS_InstallHandler(PORTC_IRQn, PORTC_ISR, (isr_t*) 0);
	INT_SYS_EnableIRQ(PORTC_IRQn);

	error = LPUART_DRV_Init(&UART1,&lpUartState1, &lpuart_1_InitConfig0);
	DEV_ASSERT(error == STATUS_SUCCESS);

//	LED_RED
//	PINS_DRV_SetPins(LED_RED, 1 << LED_RED_PIN);
	PINS_DRV_ClearPins(GPIO_OUT_PORT, 1 << GPIO_OUT_PIN);

	while (1) {
//		delay(720000);
		printf("Count status : %d\n", count);

		switch (count) {
		case 0:
			PINS_DRV_ClearPins(LED0_PORT, 1 << LED0_PIN);
			PINS_DRV_ClearPins(LED1_PORT, 1 << LED1_PIN);
			PINS_DRV_ClearPins(LED2_PORT, 1 << LED2_PIN);
			break;

		case 1:
			PINS_DRV_SetPins(LED0_PORT, 1 << LED0_PIN);
			PINS_DRV_ClearPins(LED1_PORT, 1 << LED1_PIN);
			PINS_DRV_ClearPins(LED2_PORT, 1 << LED2_PIN);
			break;

		case 2:
			PINS_DRV_ClearPins(LED0_PORT, 1 << LED0_PIN);
			PINS_DRV_SetPins(LED1_PORT, 1 << LED1_PIN);
			PINS_DRV_ClearPins(LED2_PORT, 1 << LED2_PIN);
			break;

		case 3:
			PINS_DRV_ClearPins(LED0_PORT, 1 << LED0_PIN);
			PINS_DRV_ClearPins(LED1_PORT, 1 << LED1_PIN);
			PINS_DRV_SetPins(LED2_PORT, 1 << LED2_PIN);
			break;

		default:
			break;
		}

//		PINS_DRV_TogglePins(GPIO_OUT_PORT, 1 << GPIO_OUT_PIN);
	}
	return exit_code;
}

/* END main */
/*!
 ** @}
 */

 

Error messages

make: *** [makefile:48: test.elf] Error 1
multiple definition of `CLOCK_DRV_GetFreq'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:1859: first defined here
multiple definition of `CLOCK_DRV_GetSystemClockSource'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/scg_hw_access.h:72: first defined here
multiple definition of `CLOCK_DRV_Init'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:602: first defined here
multiple definition of `CLOCK_DRV_SetClockSource'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4014: first defined here
multiple definition of `CLOCK_DRV_SetModuleClock'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:3394: first defined here
multiple definition of `CLOCK_DRV_SetSystemClock'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:3549: first defined here
multiple definition of `CLOCK_SYS_GetCurrentConfiguration'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4242: first defined here
multiple definition of `CLOCK_SYS_GetErrorCallback'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4256: first defined here
multiple definition of `CLOCK_SYS_GetFreq'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4275: first defined here
multiple definition of `CLOCK_SYS_Init'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4092: first defined here
multiple definition of `CLOCK_SYS_SetConfiguration'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4287: first defined here
multiple definition of `CLOCK_SYS_UpdateConfiguration'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/clock/S32K1xx/clock_S32K1xx.c:4123: first defined here
multiple definition of `INT_SYS_ClearPending'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:439: first defined here
multiple definition of `INT_SYS_DisableIRQ'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:225: first defined here
multiple definition of `INT_SYS_DisableIRQGlobal'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:271: first defined here
multiple definition of `INT_SYS_EnableIRQ'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:196: first defined here
multiple definition of `INT_SYS_EnableIRQGlobal'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:248: first defined here
multiple definition of `INT_SYS_GetActive'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:513: first defined here
multiple definition of `INT_SYS_GetPending'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:491: first defined here
multiple definition of `INT_SYS_GetPriority'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:366: first defined here
multiple definition of `INT_SYS_InstallHandler'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:114: first defined here
multiple definition of `INT_SYS_SetPending'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:459: first defined here
multiple definition of `INT_SYS_SetPriority'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/interrupt/interrupt_manager.c:301: first defined here
multiple definition of `PINS_DRV_ClearPinIntFlagCmd'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:216: first defined here
multiple definition of `PINS_DRV_ClearPins'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:285: first defined here
multiple definition of `PINS_DRV_ClearPortIntFlagCmd'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:284: first defined here
multiple definition of `PINS_DRV_ConfigDigitalFilter'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:258: first defined here
multiple definition of `PINS_DRV_DisableDigitalFilter'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:245: first defined here
multiple definition of `PINS_DRV_EnableDigitalFilter'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:232: first defined here
multiple definition of `PINS_DRV_GetPinIntSel'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:200: first defined here
multiple definition of `PINS_DRV_GetPinsDirection'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:67: first defined here
multiple definition of `PINS_DRV_GetPinsOutput'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:237: first defined here
multiple definition of `PINS_DRV_GetPortInputDisable'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:149: first defined here
multiple definition of `PINS_DRV_GetPortIntFlag'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:272: first defined here
multiple definition of `PINS_DRV_Init'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.c:54: first defined here
multiple definition of `PINS_DRV_ReadPins'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:330: first defined here
multiple definition of `PINS_DRV_SetGlobalIntControl'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.c:307: first defined here
multiple definition of `PINS_DRV_SetGlobalPinControl'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.c:290: first defined here
multiple definition of `PINS_DRV_SetMuxModeSel'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.c:90: first defined here
multiple definition of `PINS_DRV_SetPinDirection'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.c:225: first defined here
multiple definition of `PINS_DRV_SetPinIntSel'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:169: first defined here
multiple definition of `PINS_DRV_SetPins'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:262: first defined here
multiple definition of `PINS_DRV_SetPinsDirection'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:110: first defined here
multiple definition of `PINS_DRV_SetPortInputDisable'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:131: first defined here
multiple definition of `PINS_DRV_SetPullSel'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.h:96: first defined here
multiple definition of `PINS_DRV_TogglePins'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:307: first defined here
multiple definition of `PINS_DRV_WritePin'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.c:471: first defined here
multiple definition of `PINS_DRV_WritePins'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_driver.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_gpio_hw_access.h:214: first defined here
multiple definition of `PINS_Init'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.c:135: first defined here
multiple definition of `PINS_SetGlobalIntControl'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.c:380: first defined here
multiple definition of `PINS_SetGlobalPinControl'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.c:351: first defined here
multiple definition of `PINS_SetMuxModeSel'; ./SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.o:/root/workspaceS32DS.3.5/test/Release_FLASH/../SDK/S32K146_SDK_4.0.1/platform/drivers/src/pins/pins_port_hw_access.c:298: first defined here

 

0 项奖励
回复
3 回复数

9,456 次查看
zubizeratta
Contributor II

Seems like you are including the SDK folders twice.  You could try again after you remove the one in the project folder

标记 (1)
0 项奖励
回复

9,417 次查看
AbhijithKannan
Contributor II

That's seems to be the case. When I add lpuart driver using peripheral menu in code configuration, a new folder called platform is created containing the same drivers present in the S32K146_SDK_4.0.1 folder. But I don't understand why it creating two driver codes.

0 项奖励
回复

9,414 次查看
AbhijithKannan
Contributor II

S32K146_SDK_4.0.1 folder is having a drivers folder containing the drivers for clock, interrupt and pins and a device folder having startup code and other files. The platform folder only have the drivers folders which contains the drivers for clock , interrupt, pins, edma and lpuart.

I deleted the drivers folder present in the S32K146_SDK_4.0.1 to check if that could resolve the issue. At first compile it gave me a build error but when I compiled it again without making any changes it compiled successfully. So then run the code in debug and got the error given below

No source available for "WDOG_EWM_IRQHandler() at 0x458"

0 项奖励
回复