Multilink connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,815件の閲覧回数
whinojo
Contributor II

Good evening, I need some help in finding out how to connect the PE micro Multilink Universal to my s32K144 EVB board. I have search everywhere with no luck. In the board there are 2 identical connectors one marked as SWD and the other SDA that fit the Multilink ribbon connector. Can I connect to either, this doesn't seem clear from the documentation.

Thank you in advance for your help.

Regards.

0 件の賞賛
返信
1 解決策
5,802件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi whinojo,

J14 of S32K144EVB should be used to connect external PEMicro Multilink(PORT G).

J14 S32K144EVB PORT G PEMicro Multilink.pngJ14 S32K144EVB PORT G PEMicro Multilink.png

元の投稿で解決策を見る

4 返答(返信)
5,578件の閲覧回数
Dipen
Contributor I

In NXP website it is mentioned PE Micro Multilink Universal supports S32K144, but my supplier says to go with PE Micro Multilink Universal FX. So can I use either of them to program the microcontroller?

0 件の賞賛
返信
5,792件の閲覧回数
whinojo
Contributor II

Thank you all for the quick reply. Highly appreciated. Best regards.

0 件の賞賛
返信
5,803件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi whinojo,

J14 of S32K144EVB should be used to connect external PEMicro Multilink(PORT G).

J14 S32K144EVB PORT G PEMicro Multilink.pngJ14 S32K144EVB PORT G PEMicro Multilink.png

5,812件の閲覧回数
KalaimaniArumugamdev
Contributor III

hi,

   First thing s32K144 EVB board have own on-board open SDA MCU. Via USB connector to you can program and debug you board.https://www.pemicro.com/downloads/download_file.cfm?download_id=376  

  Otherwise PE micro Multilink Universal port G is match with s32K144 EVB board SWD port you can use this for program and debug.https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB