Missing .elf Files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,475件の閲覧回数
SalomonD
Contributor I

Hey All,
I recently bought the S32K116 Development Kit and wanted to get started using the code examples provided by the Motor Control Software. However, while setting everything up, I noticed the .elf file for the debugger was missing in my installation files.
My question would be, if there is a database where I can get the code examples from NXP directly. I tried reinstalling each software needed for the development board, but the files were still missing. There were no error messages during installation and I can open the software just fine. It's just missing the .elf file.

Help would be much appreciated

タグ(1)
0 件の賞賛
返信
1 解決策
2,464件の閲覧回数
yash_bhatnagar9
Contributor II

You can download the S32DS software from here "https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-REFSW-D"

yash_bhatnagar9_0-1683025594316.png

After installing you can open the S32DS and install/update the extensions related to S32K1XX and the you can choose a example project by going to 

yash_bhatnagar9_1-1683026005911.png

You can also try to download the RTD for S32K1XX . It has example projects as well.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,465件の閲覧回数
yash_bhatnagar9
Contributor II

You can download the S32DS software from here "https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-REFSW-D"

yash_bhatnagar9_0-1683025594316.png

After installing you can open the S32DS and install/update the extensions related to S32K1XX and the you can choose a example project by going to 

yash_bhatnagar9_1-1683026005911.png

You can also try to download the RTD for S32K1XX . It has example projects as well.

 

 

0 件の賞賛
返信