Method to re-generate a Single PWM pulse (S32K312 eMIOS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Method to re-generate a Single PWM pulse (S32K312 eMIOS)

1,876 Views
CCY_Yu
Contributor I

Hi, NXP:

    Reference to post: https://community.nxp.com/t5/S32K/How-to-Generate-a-Single-PWM-Period-and-Stop-S32K312-eMIOS/m-p/209...

We observed that after calling Emios_Pwm_Ip_InitChannel(), the PWM pulse was successfully generated, and an interrupt event was triggered. However, it seems that the callback function subsequently disabled the interrupt notification.
It look like it could generate a single pulse as well.

We would like to understand the correct procedure for generating the PWM pulse again. Specifically:

Is it appropriate to call Emios_Pwm_Ip_InitChannel() again to re-trigger the single pulse?

Or is there an alternative API that should be used to restart pulse generation and re-enable the interrupt?

We would appreciate your clarification on the recommended approach for re-generating the pulse after the initial trigger.

Tags (1)
0 Kudos
Reply
5 Replies

1,819 Views
CCY_Yu
Contributor I

Dear NXP Support Team,

Thank you for your feedback.

Based on your previous sample procedure, we are now able to generate a single pulse using the eMIOS module.

We have currently configured the pulse period to 10 seconds, and the output seems to behave as expected in terms of signal generation.

However, we have observed that the interrupt callback function is triggered twice, 

Could you please help us check:

  1. Is this behavior expected under DAOC or the current mode used?

  2. Are there any recommended steps to ensure that the callback is only triggered once per pulse?

Thank you for your continued support.

 

CCY_Yu_0-1747808629049.pngCCY_Yu_1-1747808653411.png

 

0 Kudos
Reply

1,797 Views
_Leo_
NXP TechSupport
NXP TechSupport

I would have to debug your project to give you a proper answer.

0 Kudos
Reply

1,780 Views
CCY_Yu
Contributor I

Hi, NXP:

   Please help to check the project, thanks.

0 Kudos
Reply

1,554 Views
_Leo_
NXP TechSupport
NXP TechSupport

Please check your email.

0 Kudos
Reply

1,835 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

For a second (or more pulses) you should call Emios_Pwm_Ip_InitChannel() and Emios_Pwm_Ip_SetFlagRequest() functions.

Please find attached project.

It use another eMIOS channel performing GPT in one-shot mode to generate a second DAOC pulse after 100ms:

_Leo__0-1747780760686.png

Or in continuous mode every 100ms:

_Leo__1-1747780776508.png

Hope it helps!

0 Kudos
Reply