Mcl Limitations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mcl Limitations

1,842 Views
NermeenShaban
Contributor I

for s32k388 :

I need to use 10 Flexio channels for UART and I2C 

so I need 10 MCL channels but I have limitations of MCL channels (8 channels only)

so Is it mean I can use 8 channels of Flexio only ? 

0 Kudos
Reply
2 Replies

1,803 Views
john_floros
NXP Employee
NXP Employee

Hello,

Below is the number of timers and shift registers available on the FlexIO peripheral on the S32K388.  The number of pins that the FlexIO has access to is 32 but it does not represent the number of timers and registers that are available.

john_floros_0-1706889556751.png

 

Regards,

John

0 Kudos
Reply

1,824 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @NermeenShaban,

Currently, the driver supports only channels 0 through 7 for FlexIO, even though the reference manual states the 32 FlexIO channels:

Julin_AragnM_2-1706722692742.png

 

Julin_AragnM_3-1706722696909.png

The drivers may not encompass the whole limitations of the MCU, for which further implementation must be based on the client's side.

Best regards,
Julián.

0 Kudos
Reply