Mcal Can module product configuration code failed using s32ds configure tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mcal Can module product configuration code failed using s32ds configure tool

911 次查看
laofu
Contributor II

Hi,@NXP

I use s32ds to comfigure a Mcal CAN module,and RTD vesion is 1.0.1,but when i product the code,there is several error warnning as the following picture show.then I found the producted file FlexCAN_Ip_Cfg.h is empty and the project build failed.in addition, when I import the Can_example_S32K144 example project and it work well. can you help me, thanks very much

laofu_0-1679535890474.png

laofu_1-1679536103567.png

 

 

0 项奖励
回复
1 回复

797 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry for long delay, did you solved the issue? 

0 项奖励
回复