Max safe output current allowed for each GPIO on S32K144-EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max safe output current allowed for each GPIO on S32K144-EVB

ソリューションへジャンプ
1,080件の閲覧回数
Teo25
Contributor I

Hello,

 

I just acquired a dev board S32K144-EVB, so i'm quite new to this MCU.

I have some questions regarding the maximum output current that can be provided through 1 GPIO pin without the risk of damage to the pin.

From the data sheet it says that max current for a GPIO pin is 5mA, but at the same time, if DSE function is enabled on the output driver of said pin, than the maximum current  can be increased to 20 mA max.

 
 

From the documentation provided by NXP, the DSE function can function  as a series resistance between output and load.

What I understand from this is that the Output driver of each GPIO can act  also as a current limit , and prevent the load from drawing too much current and damaging the pin, or some current limiting resistor is still needed to prevent the load from drawing more current than the limit?

 

Thank you in advance for support.

0 件の賞賛
返信
1 解決策
1,027件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3 返答(返信)
1,037件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Values that you mention are minimum values, not maximum. There is no max spec for an individual GPIO.

For maximum current please refer to IOHT, it is for all ports.

2025-02-27_12-10-16.png

Hope it helps you.

Have a nice day!

0 件の賞賛
返信
1,032件の閲覧回数
Teo25
Contributor I

Thank you for the response.

 

So this means that with no max value for current, even with no DSE activated, i can draw for example  even up to 20mA on a single GPIO without physical damage to the respective pin on the long term? All as long as I do not exceed combined 100mA on all pins combined.

 

タグ(3)
0 件の賞賛
返信
1,028件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

It is correct.

0 件の賞賛
返信