Master Key

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,027件の閲覧回数
youxi
Contributor IV

Hello:

I have had two problems:

Is it NVM KEY after Master key is loaded?

Does ad update Master key need to know the original Master key?

タグ(1)
0 件の賞賛
返信
1 解決策
3,018件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @youxi 

"Is it NVM KEY after Master key is loaded?"

- I'm sorry, I'm not sure if I can understand this question. Please try to reformulate it.

"Does ad update Master key need to know the original Master key?"

- Yes, it is required by SHE specification. You need to know the counter as well.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,019件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @youxi 

"Is it NVM KEY after Master key is loaded?"

- I'm sorry, I'm not sure if I can understand this question. Please try to reformulate it.

"Does ad update Master key need to know the original Master key?"

- Yes, it is required by SHE specification. You need to know the counter as well.

Regards,

Lukas

0 件の賞賛
返信
2,966件の閲覧回数
youxi
Contributor IV
Hi @lukaszadrapa
The index number of the counter is from 0 to 15. what does this index number represent. and whether the super user permission is required to read the counter value.
0 件の賞賛
返信
2,961件の閲覧回数
youxi
Contributor IV

This is the copied function in demo app but I can`t read the value to the counter

youxi_0-1689128424151.png

youxi_1-1689128448167.png

youxi_2-1689128465388.png

 

 

0 件の賞賛
返信
2,942件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

This is something completely different.

SHE specification defines that each NVM key has a counter and it must be incremented for each update of a key. The keys can't be exported (RAM plain key is an exception) and also it is not possible to read the counter. It's up to user to know what the current counter is.

Mentioned monotonic counter is different feature. There are 16 monotonic counters (so index 0-15 is used to address them). It's not a feature related to SHE commands.

Regards,

Lukas

0 件の賞賛
返信