MTRDEVKSPNK144 Compiler error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MTRDEVKSPNK144 Compiler error

3,210 Views
sunnywu
Contributor II

hi

when I compiler  C:\NXP\MC_DevKits\MTRDEVKSPNK144\sw\MTRDEVKSPNK144_S32DS   project  use the S32DS.2018.R1, it always remind me that 

Cannot run program "": Launching failed
Error: Program "" not found in PATH
PATH=[C:/NXP/S32DS.2018.R1/eclipse/jre/bin/server;C:/NXP/S32DS.2018.R1/eclipse/jre/bin;C:/NXP/S32DS.2018.R1/eclipse/jre/lib/amd64;C:\Program Files (x86)\RSA SecurID Token Common;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;C:\ProgramData\Oracle\Java\javapath;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files (x86)\Microchip\MPLAB C32 Suite\bin;C:\Program Files (x86)\HI-TECH Software\PICC-18\PRO\9.66\bin;C:\Program Files (x86)\HI-TECH Software\PICC-18\PRO\9.65\bin;C:\Program Files (x86)\Microchip\xc8\v1.42\bin;C:\Program Files (x86)\Microchip\xc16\v1.31\bin;C:\Program Files\Perforce;C:\Program Files (x86)\WebEx\PTools020000000;C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility;C:\Program Files\MATLAB\R2018b\bin;D:\Program Files\PuTTY\;C:\Program Files (x86)\Webex\Webex\Applications;C:\Program Files (x86)\Sennheiser\SoftphoneSDK\;C:\Users\sunnyw.wu\AppData\Local\Microsoft\WindowsApps;;C:\NXP\S32DS.2018.R1\S32DS\SA\bin;C:\NXP\S32DS.2018.R1\eclipse]
0 Kudos
Reply
3 Replies

3,072 Views
sunnywu
Contributor II

currently, I can compile the project, but when I download the file, it always reming me , please help me solved it.

0 Kudos
Reply

3,072 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

could you be more specific? Could you describe your steps and show what is not working exactly?

Thanks,

Lukas

0 Kudos
Reply

3,072 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

do you have everything up to date?

I downloaded MTRDEVKSPNK144 package from the web (version 1.4), I imported it to S32 Design Studio 2018.R1 (I have latest Update 9 installed), cleaned the project, generated the code for Processor expert and then successfully compiled...

So, first check if you have latest versions:

https://www.nxp.com/webapp/Download?colCode=MTRDEVKSPNK144_SW&appType=license 

S32 Design Studio IDE for Arm® based MCUs | NXP 

Regards,

Lukas

0 Kudos
Reply