MCTPX1AK324 Secure Debug enabled?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCTPX1AK324 Secure Debug enabled?

ソリューションへジャンプ
5,377件の閲覧回数
hns80
Senior Contributor I

I am attempting to debug the example project for the triple PMSM project an with the PE Multilink and I received this message:

Secure Debug might be enabled on this device. If so, please unlock the device via PEmicro scripts before attempting to connect again

hns80_0-1698699910262.png

 

The board is powered with 12V and the jumpers are set as specified in the getting started guide.

I don't think the board ships with secure debug enabled and the Multilink has been updated to the latest firmware. What might be causing this issue?

 

 

 

0 件の賞賛
返信
1 解決策
5,331件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @hns80 

I send you a private message.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,332件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @hns80 

I send you a private message.

0 件の賞賛
返信
5,348件の閲覧回数
hns80
Senior Contributor I

I probed the board and discovered a few things that look wrong:

1. V15 = 1.35V
2. V11 = 1.35V
3. PTA5_MCU_RESETB = 0.6V

The other voltages look OK:
VREFH = 5V
VCC_HV_A_MCU = 4.99V
VCC_HV_B_MCU = 4.99V
VBAT = 11.96V

 

0 件の賞賛
返信
5,358件の閲覧回数
hns80
Senior Contributor I

This was the first time I tried to connect. I was trying to start a debug session with the example project. 

0 件の賞賛
返信
5,368件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @hns80 

To confirm, did you upload any code to the board? Did you install HSE or modify anything in the UTES section? Or does it show this message since you received it from NXP/distributor?

 

B.R.

VaneB

 

0 件の賞賛
返信
5,351件の閲覧回数
hns80
Senior Contributor I

I did not install HSE or modify anything in the UTEST section.

I only tried to launch the predefined debug group.

 

I verified the debugger is working on another board.

 

0 件の賞賛
返信
3,851件の閲覧回数
XuanZhangming
Contributor II

Hi @hns80

I am currently facing the same problem, is there a specific solution

Thanks & Best Regards

0 件の賞賛
返信