MCTPX1AK324 Secure Debug enabled?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCTPX1AK324 Secure Debug enabled?

Jump to solution
5,390 Views
hns80
Senior Contributor I

I am attempting to debug the example project for the triple PMSM project an with the PE Multilink and I received this message:

Secure Debug might be enabled on this device. If so, please unlock the device via PEmicro scripts before attempting to connect again

hns80_0-1698699910262.png

 

The board is powered with 12V and the jumpers are set as specified in the getting started guide.

I don't think the board ships with secure debug enabled and the Multilink has been updated to the latest firmware. What might be causing this issue?

 

 

 

0 Kudos
Reply
1 Solution
5,344 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @hns80 

I send you a private message.

View solution in original post

0 Kudos
Reply
6 Replies
5,345 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @hns80 

I send you a private message.

0 Kudos
Reply
5,361 Views
hns80
Senior Contributor I

I probed the board and discovered a few things that look wrong:

1. V15 = 1.35V
2. V11 = 1.35V
3. PTA5_MCU_RESETB = 0.6V

The other voltages look OK:
VREFH = 5V
VCC_HV_A_MCU = 4.99V
VCC_HV_B_MCU = 4.99V
VBAT = 11.96V

 

0 Kudos
Reply
5,371 Views
hns80
Senior Contributor I

This was the first time I tried to connect. I was trying to start a debug session with the example project. 

0 Kudos
Reply
5,381 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @hns80 

To confirm, did you upload any code to the board? Did you install HSE or modify anything in the UTES section? Or does it show this message since you received it from NXP/distributor?

 

B.R.

VaneB

 

0 Kudos
Reply
5,364 Views
hns80
Senior Contributor I

I did not install HSE or modify anything in the UTEST section.

I only tried to launch the predefined debug group.

 

I verified the debugger is working on another board.

 

0 Kudos
Reply
3,864 Views
XuanZhangming
Contributor II

Hi @hns80

I am currently facing the same problem, is there a specific solution

Thanks & Best Regards

0 Kudos
Reply